How to solve this problem? Does the flash scrubbing have to do with it?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to solve this problem? Does the flash scrubbing have to do with it?

548件の閲覧回数
1010663655
Contributor I

We have one piece of MCU which type is SPC5748, after we have burned different programs with the Multilink Universal for it several times, we can never program successfully and it would be dying at Verifing(as shown below). How to solve this problem? Does the flash scrubbing have to do with it?

Connection from "127.0.0.1" via 127.0.0.1

Copyright 2017 P&E Microcomputer Systems,Inc.

Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -?

 

CMD>RE

 

Initializing.

MPC574xC Device detected.

Target has been RESET and is active.

CMD>CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&E\nxp_mpc5748g_1x32x1520k_cflash.pcp

 

Initializing.

MPC574xC Device detected.

Initialized.

 

;version 1.05, 06/26/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [5748G_6080k]

 

;device NXP, MPC5748G, 1x32x1520k, desc=CFlash

 

;begin_cs device=$00F90000, length=$005F0000, ram=$40000000

 

Loading programming algorithm ...

 

WARNING - Selected .PCP file has been modified. CRC16 = $5A63

Done.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00FA0000-00FA0003 ...

タグ(2)
0 件の賞賛
返信
0 返答(返信)