I have been using LPC824 (in both packages) and have found the LPC Initialization Tool useful both to produce the PinMux files, and to get a quick visualization of Pin Mapping. But moving up to the LPC845 I do not see a selection (yet) for this processor. And looking at Config Tools I do not see any LPC8xx parts supported. Are there plans for augmenting the LPC Initialization Tool to work for LPC845? And when?
Solved! Go to Solution.
Hi Norman Jones,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Norman Jones,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thankyou Jeremy:
I will continue with the approach of assigning pins with calls in the code
for this project and hope to return to the PinMap tool if it is ready in
time for the next project.
--Norm
jeremyzhou
replied to the discussion
"Re: If Config Tools does not support LPC 8xx parts, and the LPC
Initialization Tool does not (yet) recognize LPC845, how do I set up Pin
I/O and SPI SSELn pins?"
To view the discussion, visit:
https://community.nxp.com/message/954947?commentID=954947&et=watches.email.thread#comment-954947
>