Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Config Tools for IMX V15.1 on Ubuntu (22.04, 22.10, 23) fonts are gibberish

跳至解决方案
725 次查看
bowerymarc
Contributor V

Screenshot 2024-02-26 145637.png

0 项奖励
回复
1 解答
686 次查看
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
687 次查看
liborukropec
NXP Employee
NXP Employee

Hi Marc,

 

we do not see such issue, so only few hints:

  1. Ubuntu 22.10 and 23 are not supported
  2. You can try to use Xorg, instead of Wayland as Wayland is not fully compatible and supported (via small wheel during login)
    liborukropec_1-1709029799902.png

     

  3. For VirtualBox I remember similar issue, please make sure there's enough memory for the graphics card and that the compatible card is used:
    liborukropec_0-1709029710115.png

 

Regards,

Libor

0 项奖励
回复
702 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bowerymarc 

 

Here is my test result based on Ubuntu22.04.

Please make sure you have updated and upgraded the Ubuntu packages.

Zhiming_Liu_0-1708992910021.png

Best Regards

Zhiming

 

0 项奖励
回复