I'm using blhost on Ubuntu16.04 and I have made sure that all dependencies required in the manual such as libudev.so.1, libc.so.6, etc are all installed and can be found on system path. But when I run
sudo blhost -p COM1 -- get-property 1
It reports an error
"Could not open serial port.Error: UartPeripheral() cannot open PC UART port(COM1), speed(57600 Hz)."
What's the problem here?
COM ports are for Windows, try replacing "COM1" with /dev/ttyUSB0 or /dev/ttyAMC0 depending on the output of
ls /dev/tty*
Hi Mike,
I used the board we developed ourselves with the K64F12.
and i'm sure there is no problem with the board.because i was successful on win7 systems .
Hi,
Sorry for the later reply.
Which board you are using with KBOOT blhost tool?
Thanks with regards,
Mike
Hi Mike,
I used the board we developed ourselves with the K64F12.
and i'm sure there is no problem with the board.because i was successful on win7 systems .