Hello,
已解决! 转到解答。
1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.
AN12218: S32K1xx Bootloader – Application Note
AN12323: S32K1xx Firmware updates – Application Note
2. MCUXpresso IDE has nothing to do with S32K.
1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.
AN12218: S32K1xx Bootloader – Application Note
AN12323: S32K1xx Firmware updates – Application Note
2. MCUXpresso IDE has nothing to do with S32K.