sending 10Gb/s traffic to 25Gb/s ports

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sending 10Gb/s traffic to 25Gb/s ports

Jump to solution
1,152 Views
LeNormich
Contributor I

Hello,

I want to use an LS2088 board as a traffic generator toward an LX2160 board.

No issue when using copper between LS2088 and LX2160 1Gb/s and 10Gb/s ports.

For a use case, I would like to generate traffic to LX2160 25Gb/s ports (SFP+ / fiber). The problem is that when connecting the two boards, LX2160 always indicates the 25 Gb/s ports as DOWN and NO-CARRIER.
I suppose this is due to (absence of?) speed negociation between the ports. 

So my question is: can LX2160 receive  10Gb/s traffic on the 25Gb/s ports? is there a way to configure that?

Thanks,

Regards,

 

0 Kudos
Reply
1 Solution
1,148 Views
ufedor
NXP Employee
NXP Employee

> can LX2160 receive 10Gb/s traffic on the 25Gb/s ports?

The LX2160A 25G Ethernet port can be connected only to another 25G Ethernet port.

 

View solution in original post

0 Kudos
Reply
2 Replies
1,149 Views
ufedor
NXP Employee
NXP Employee

> can LX2160 receive 10Gb/s traffic on the 25Gb/s ports?

The LX2160A 25G Ethernet port can be connected only to another 25G Ethernet port.

 

0 Kudos
Reply
1,133 Views
LeNormich
Contributor I

Thanks for the reply.

Is there a rationale for that?

Tags (1)
0 Kudos
Reply