fsl_fman_ucode_ls1043_r1.0_108_4_9.bin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fsl_fman_ucode_ls1043_r1.0_108_4_9.bin

Jump to solution
1,900 Views
zumengchen
Contributor III

Hi experts,

This fman file has been mentioned in QorIQ SDK 2.0 Documentation, Rev. 0, May 2016, which is 4.4.5.4 Frame Manager Microcode (FMan ucode). but I can't find it in QorIQLinuxSDKv2.0AARCH64IMAGE.iso, there are only the following two fman bin file:

ls1043ardb/fsl_fman_ucode_t2080_r1.1_106_4_18.bin

ls1043ardb/fsl_fman_ucode_t2080_r1.1_108_4_5.bin

The weird thing is the name here, why t2080?

I using this fman ucode, Mini-PCIe can't be seen. Something wrong, can you help me out, thanks a lot.

Cheers,

Zumeng

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,457 Views
ufedor
NXP Employee
NXP Employee

> The weird thing is the name here, why t2080?

These SOCs (T2080 and LS1043A) have the same FMan IP and share the same microcode.

> I using this fman ucode, Mini-PCIe can't be seen.

PCIe controller is completely independent of the FMan and its microcode.

View solution in original post

0 Kudos
Reply
2 Replies
1,457 Views
zumengchen
Contributor III

Thanks a lot, good to know

0 Kudos
Reply
1,458 Views
ufedor
NXP Employee
NXP Employee

> The weird thing is the name here, why t2080?

These SOCs (T2080 and LS1043A) have the same FMan IP and share the same microcode.

> I using this fman ucode, Mini-PCIe can't be seen.

PCIe controller is completely independent of the FMan and its microcode.

0 Kudos
Reply