Hi experts,
This fman file has been mentioned in QorIQ SDK 2.0 Documentation, Rev. 0, May 2016, which is 4.4.5.4 Frame Manager Microcode (FMan ucode). but I can't find it in QorIQLinuxSDKv2.0AARCH64IMAGE.iso, there are only the following two fman bin file:
ls1043ardb/fsl_fman_ucode_t2080_r1.1_106_4_18.bin
ls1043ardb/fsl_fman_ucode_t2080_r1.1_108_4_5.bin
The weird thing is the name here, why t2080?
I using this fman ucode, Mini-PCIe can't be seen. Something wrong, can you help me out, thanks a lot.
Cheers,
Zumeng
已解决! 转到解答。
> The weird thing is the name here, why t2080?
These SOCs (T2080 and LS1043A) have the same FMan IP and share the same microcode.
> I using this fman ucode, Mini-PCIe can't be seen.
PCIe controller is completely independent of the FMan and its microcode.
> The weird thing is the name here, why t2080?
These SOCs (T2080 and LS1043A) have the same FMan IP and share the same microcode.
> I using this fman ucode, Mini-PCIe can't be seen.
PCIe controller is completely independent of the FMan and its microcode.