LX2160A boot loader location

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A boot loader location

ソリューションへジャンプ
1,593件の閲覧回数
dmitri_lechtchinski
Contributor III

Hello,

Which devices can be used for loading boot loader image from on SoC startup? (XSPI, ...?)

Can an image be loaded from NVMe device?

Thanks,
Dmitri

0 件の賞賛
返信
1 解決策
1,589件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.

元の投稿で解決策を見る

1 返信
1,590件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.