LX2080A XSPI_A interface topology inquire

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LX2080A XSPI_A interface topology inquire

336 次查看
Rex4_Huang
Contributor I

Hi Sir,

I have two SPI devices on our board,

one is an XSPI flash for NXP U-BOOT & KERNAL use, and the other one is a QSPI device.  

Q1.Can I use XSPI_A of LX2080A to connect them?

Q2. Can these devices be worked together?

the simple connection topology is shown as below:

Rex4_Huang_0-1705634472875.png

 

0 项奖励
回复
1 回复

285 次查看
yipingwang
NXP TechSupport
NXP TechSupport

A1. The connection looks fine. However, the SW need to know one is 8 bit data line vs 4 data lines.
A2. I do not know what do you mean whether these devices can be worked together? The commands send to these two flashes should be different as one should be x8 another should be x4.

0 项奖励
回复