LX2160ARDB - How to update MC firmware, DPC, and DPL images on SD/eMMC card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160ARDB - How to update MC firmware, DPC, and DPL images on SD/eMMC card

LX2160ARDB - How to update MC firmware, DPC, and DPL images on SD/eMMC card

Follow these steps to update the DPAA2 MC firmware, DPC, and DPL images for the LX2160ARDB on the SD/eMMC card. 

Below steps are valid for both LX2160ARDB Rev 1.0 and Rev 2.0 revisions.

Compiling MC firmware

  1. Clone the qoriq-mc-binary repository.

    git clone https://github.com/NXP/qoriq-mc-binary.git

  2. $ cd qoriq-mc-binary/lx2160a/
  3. $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-20.04

The prebuilt MC firmware image, mc_10.20.4_lx2160a.itb, is available at qoriq-mc-binary/lx2160a/.

Note: The exact name of the MC firmware image may vary depending on the LSDK release version used.                 

Compiling DPC and DPL images

  1. Clone the mc-utils repository and compile the DPC and DPL images.

    git clone https://source.codeaurora.org/external/qoriq/qoriq-components/mc-utils

  2. cd mc-utils/
  3. $ git checkout LSDK-<LSDK version>. For example, $ git checkout LSDK-20.04
  4. If required, make changes to the DPC and DPL files.
  5. make -C config/

The compiled dpc-usxgmii.dtb and dpl-eth.19.dtb images are available at /mc-utils/config/lx2160a/RDB/.

Note: The exact name of the DPL and DPC images may vary depending on the LSDK release version used.            

SD/eMMC card start block number for MC, DPL, and DPC images

Image  SD/eMMC card start block number
DPAA2 MC firmware 0x05000 = 20480
DPAA2 DPL  0x06800 = 26624
DPAA2 DPC 0x07000 = 28672

 

Refer the LSDK firmware and SD card start block number for complete listing of the SD card start block numbers for all LSDK firmware images.   

Programming MC, DPC, and DPL images to SD/eMMC card

Boot LX2160ARDB from FlexSPI. Ensure that the switches are set to boot the board from FlexSPI.

  • SW1[1:8] = 1111 1000
  • SW2[1:8] = 0000 0110
  • SW3[1:8] = 1111 1100
  • SW4[1:8] = 1011 1000

Boot from FlexSPI NOR flash0: => qixis_reset

For example:

For LX2160ARDB, in U-Boot log, you’ll see:

Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from FlexSPI DEV#0

Set up Ethernet connection

When board boots up, U-Boot prints a list of enabled Ethernet interfaces.

DPMAC2@xlaui4, DPMAC3@xgmii, DPMAC4@xgmii, DPMAC5@25g-aui, DPMAC6@25g-aui, DPMAC17@rgmii-id, DPMAC18@rgmii-id 

 

  1. Set server IP address to the IP address of the host machine on which you have configured the TFTP server. 

    => setenv serverip <ipaddress1>

  2. Set ethact and ethprime as the ethernet interface connected to the TFTP server.

    NOTE: See LX2160ARDB Ethernet Port Mapping for the mapping of Ethernet port names appearing on the chassis front panel with the port names in U-Boot and Linux.

    => setenv ethprime <name of interface connected to TFTP server>

    For example:

    => setenv ethprime DPMAC3@xgmii 

    => setenv ethact <name of interface connected to TFTP server>

    For example:

    => setenv ethact DPMAC3@xgmii 

  3. Set IP address of the board. You can set a static IP address or, if the board can connect to a dhcp server, you can use the dhcp command. 

    Static IP address assignment:
    => setenv ipaddr <ipaddress2>
    => setenv netmask <subnet mask>

    Dynamic IP address assignment:
    => dhcp

  4. Save the settings.

          => saveenv

  5. Check the connection between the board and the TFTP server.

    => ping $serverip

    Using DPMAC3@xgmii device

    host 192.168.2.1 is alive

 Load images from TFTP server

  1. Flash MC firmware (mc_10.20.4_lx2160a.itb):

    => tftp 82000000 mc_10.20.4_lx2160a.itb

    •  Flash MC firmware to SD card:

      => mmc dev 0; mmc write 8200000 5000 <blk_cnt>

    •  Flash MC firmware to eMMC card:

      => mmc dev 1; mmc write 8200000 5000 <blk_cnt>

      Here, blk_cnt refers to number of blocks in SD/eMMC card that need to be written as per the file size.

      For example, when you load mc_10.20.4_lx2160a.itb from the TFTP server, if the bytes transferred is 1092272 (10aab0 hex), then blk_cnt is calculated as "1092272 /512 = 2133 (855 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 10 (A hex) sectors, for this example, mmc write command will be: 

      => mmc write 82000000 5000 85F

  2. Flash DPAA2 DPL image.

    => tftp 82000000 dpl-eth.19.dtb

    • Flash DPL image to SD card:

      => mmc dev 0; mmc write 8200000 6800 <blk_cnt>

    •    Flash DPL image to eMMC card:

      => mmc dev 1; mmc write 8200000 6800 <blk_cnt>

      Here, blk_cnt refers to number of blocks in SD/eMMC card that need to be written as per the file size.

      For example, when you load dpl-eth.19.dtb from the TFTP server, if the bytes transferred is 4583 (11e7 hex), then blk_cnt is calculated as "4583/512 = 8 (8 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 18 (12 hex) sectors, for this example, mmc write command will be: 

      => mmc write 82000000 6800 12

  3. Flash DPAA2 DPC image.

       => tftp 82000000 dpc-usxgmii.dtb 

    • Flash DPC image to SD card:

      => mmc dev 0; mmc write 8200000 7000 <blk_cnt>

    • Flash DPC image to eMMC card:

      => mmc dev 1; mmc write 8200000 7000 <blk_cnt>

    Here, blk_cnt refers to number of blocks in SD card that need to be written as per the file size.

    For example, when you load dpc-usxgmii.dtb from the TFTP server, if the bytes transferred is 736 (2e0 hex), then blk_cnt is calculated as "736/512 = 1 (1 hex)" + "few sectors for rounding up so that last block is not missed". So, if you round up by 11 (B hex) sectors, for this example, mmc write command will be: 

    => mmc write 82000000 7000 B

  4. Boot the board.
    • Boot from SD card: => qixis_reset sd
    • Boot from eMMC card: => qixis_reset emmc

LX2160ARDB will boot with updated MC firmware and DPC and DPL images. In the U-Boot log, you will see:

 

Model: NXP Layerscape LX2160ARDB Board

Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from SD

...

...

fsl-mc: Booting Management Complex ... SUCCESS

fsl-mc: Management Complex booted (version: 10.20.4, boot status: 0x1)

Hit any key to stop autoboot:  0

=>

 

OR

 

Model: NXP Layerscape LX2160ARDB Board

Board: LX2160ACE Rev2.0-RDB, Board version: B, boot from eMMC

...

...

fsl-mc: Booting Management Complex ... SUCCESS

fsl-mc: Management Complex booted (version: 10.20.4, boot status: 0x1)

Hit any key to stop autoboot:  0

=>

No ratings
Version history
Last update:
‎10-22-2020 12:06 AM
Updated by: