Content originally posted in LPCWare by Peter on Wed Oct 24 04:41:13 MST 2012
Hello,
I upgrade my LPCXpresso from "LPCXpresso v4.1.5 Build 219" to "LPCXpresso v4.3.0 Build 1023", and now I cannot run and debug my code which worked well with the previous version...
This is what happens : when I click the debug button, the compilation works fine, then it seems that the firmware is downloaded in my LPC1754 with the LPC-link probe and then I cannot click on the button "resume", and I don't see the first line of my code colored as usual. The only button I can click on is the "Terminate" button.
Also I must tell that I needed to "patch" the file "msys-1.0.dll" to make the compilation working.
Then I tried to reinstall LPCXpresso Build 219, but now the behaviour is the same as the Build 1023.
Please Help.
Thank you.
Peter