LPCXpresso v8.2.0_647 - cannot find -lCMSISv1p30_LPC17xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso v8.2.0_647 - cannot find -lCMSISv1p30_LPC17xx

1,807 Views
jakubpapuga-sza
Contributor II

Hi all,

I downloaded and installed LPCXpresso v8.2.0_647 and with built-in LPCXpresso programmer/probe is eveything OK.

For sure I downloaded into the LPC1769 microcontroller a *.axf file with my firmware and it works great.

 

But there is smal problem:

When I open my previous software project + CMSISv1p30_LPC17xx (as a project into a workspace) and I click the "Build" icon then the LPCXpresso console return me an error:

08:06:07 **** Incremental Build of configuration Debug for project PCBTest_FW06 ****
make -r all
Building target: PCBTest_FW06.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -L"D:\LPCXpresso_8.2.0_647 - workspace\CMSISv1p30_LPC17xx\Debug" -Xlinker -Map=PCBTest_FW06.map -Xlinker --gc-sections -mcpu=cortex-m3 -mthumb -T "PCBTest_FW06_Debug.ld" -o "PCBTest_FW06.axf" ./src/cr_startup_lpc175x.o ./src/main.o ./source/adc_ads8326.o ./source/adcbasic.o ./source/flash_memory_spi.o ./source/lcd_1.o ./source/lcd_2.o ./source/pwmbasic.o ./source/ssp.o ./source/ssp1.o ./source/timerbasic.o ./source/uartbasic.o -lCMSISv1p30_LPC17xx
c:/nxp/lpcxpresso_8.2.0_647/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/5.3.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -lCMSISv1p30_LPC17xx
collect2.exe: error: ld returned 1 exit status
make: *** [PCBTest_FW06.axf] Error 1

08:06:08 Build Finished (took 573ms)

I added CMSIS v1.30 libraries into CMSISv1p30_LPC17xx project as I show below (libraries added by me are marked in red rectangles):

Screen+01.JPG

and it does not help... The error still occurs during Building.

What should I do in this case?

4 Replies

1,088 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Sounds like you have not built the library project, or potentially not built the right build configuration. For more information see: https://community.nxp.com/message/630712 

Regards,

LPCXpresso Support

0 Kudos
Reply

1,088 Views
jakubpapuga-sza
Contributor II

Hello again,

I tried to do all things to fix the "cannot find library" error but with no results.

I downloaded and installed the lastest version of LPCXpresso - v8.2.2_650. I opened simultaneously my previous (old) LPCXpresso - v6.0.2_151 (works great) and the new LPCXpresso v8.2.2_650 (cannot find the library CMSIS).

In both LPCXpressos I opened the same project and I opened "Menu -> Project -> Properties" and I compared 3 positions of settings:

- "C/C++ Build -> Settings -> Tool Settings -> MCU C Compiler -> Includes -> Includes paths (-I)" - in "Debug" and "Release" configuration,

- "C/C++ Build -> Settings -> Tool Settings -> MCU Linker -> Libraries -> Libraries (-I)" - in "Debug" and "Release" configuration,

- "C/C++ General -> Paths and Symbols -> Includes -> Additional Assembly  Source Files + Assembly + GNU C" - in "Debug" and "Release" configuration,

I compared this settings between old LPCXpresso (v6.0.2_151) and new LPCXpresso (v8.2.2_650) and I configured LPCXpresso v8.2.2_650 exactly in the same way as old LPCXpresso (v6.0.2_151) and it gives no results - "cannot find library CMSIS" sitll exists.

Below I send a screens of my old and new LPCXpresso software libraries in the projects.

01. Old LPCXpresso (v6.0.2_151):

01. LPCXpresso v6.0.2_151 - Included libriaries.jpg

02. New LPCXpresso (v8.2.2_650):

02. LPCXpresso v8.2.2_650 - Included libriaries.jpg

 

I also followed the steps according to Creating and Linking to Library Projects "Manually creating links to library projects" but it also did not give any positive results.

Is there any way to fix this error?

I will be very grateful for your help.

0 Kudos
Reply

1,088 Views
jakubpapuga-sza
Contributor II

Hi again,

I fixed the problem and the solution was not the settings in the Menu -> Project -> Properties -> so on so on... but there was some issue with teh core_cm3.c file: CMSISv1p30_LPC13xx cannot be build in LPCXpresso IDE ver.7 | www.LPCware.com 

Please let me give some feedback answer about the "&" character in this file and differences between LPCXpresso 8.2 and the older one LPCXpresso 6.0.

Best regards,

Jakub

0 Kudos
Reply

1,088 Views
avt
Contributor III

Afaik, it was a bug in that version of cmsis.it was fixed in v2 of cmsis. I guess you could say there was a bug in earlier versions of the compiler in that they did not report the bug/error.