XIP perfomrance versus internal FLASH in LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XIP perfomrance versus internal FLASH in LPC546xx

1,582件の閲覧回数
Jetcitycowboy
NXP Employee
NXP Employee

Do you know how the execution time of the XIP (execute in place) feature of SPIFI on the LPC546xx parts would compare to  internal flash and also to the MK22FN512 executing code from internal flash?

ラベル(1)
0 件の賞賛
返信
1 返信

1,279件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kenneth,

You can refer to the "SPIFI Performance" section in the following presentation for more information. It compares the effective throughput for different flash types and there is a table showing the coremark performance results for the different memory locations:

https://community.nxp.com/docs/DOC-333596 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信