We have an application where we have interfaced "LPC54628J512ET180E" with SDRAM "IS42S16400J-7TLI" using EMC interface of LPC.
I have below queries regarding SDRAM interface with LPC.
Hi, Abhi,
For the LPC family including LPC54628J512ET180E, the SDRAM controller of LPC54628 routes it's data bus and address bus to fixed pads, in other words, it is impossible to swap the data pins or swap the address pins, because the address and data pins are fixed.
For the pin assignment, pls refer to Chapter 10: LPC546xx I/O pin configuration (IOCON) in UM10912.pdf, it can be downloaded from the link:
https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
Hope it can help you
BR
XiangJun Rong