Smallest programing size on LPC5500

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Smallest programing size on LPC5500

跳至解决方案
1,372 次查看
JRIIS
NXP Employee
NXP Employee

I need to understand what is the smallest bit size that can be programmed - within one operation - in internal Flash on LPC5528.

I also need to understand what is the smallest size that be erased at one operation.

This file is for collecting and store calibration data from production/test, but need to be passable to update a few times over product lifetime after reparation.

 Thanks,

/Jakob

标签 (1)
0 项奖励
回复
1 解答
1,361 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JRIIS 

It's right the minimum programming and erase size is the page size, 512 bytes. The HW decides this feature. No other option.

Hope this clarifies the issue.

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,369 次查看
JRIIS
NXP Employee
NXP Employee

I found following my self:

2.1.1 Page size and sector size

The sector size of the LPC5500 series internal flash memory is 32 KB and the page size is 512 bytes.

The minimum programming size is the page size, 512 bytes.

The minimum erase size is page size, 512 bytes

AN12949 where I found this info is attached.

This seem to be quite large potion - so if there is any tip to program smaller potion? then I like to know.

Thanks,

Jakob

0 项奖励
回复
1,362 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JRIIS 

It's right the minimum programming and erase size is the page size, 512 bytes. The HW decides this feature. No other option.

Hope this clarifies the issue.

Jun Zhang

0 项奖励
回复