Setting up LPCXpresso v8.2.2 in Ubuntu 16.10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting up LPCXpresso v8.2.2 in Ubuntu 16.10

1,454件の閲覧回数
johnygeorgemala
Contributor I

I am trying to install the LPCXpresso v8.2.2  in Ubuntu 16.10. I did everything and installed the stuffs as per the readme given.

Now I am trying to connect to a LPC824 Max board. Ubuntu detects the board. I am trying to debug a sample application and I have the following error.

LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:13:28 - crt_emu_cm_redlink build 725)
Failed on connect: Ee(36). Could not connect to core.
No connection to emulator device

How to fix it ?

タグ(2)
0 件の賞賛
返信
1 返信

1,289件の閲覧回数
converse
Senior Contributor V
0 件の賞賛
返信