Hello,
Checking the schematic of the lpcxpresso55s69 dev board, I coudn't find all the PLU_IN1 in the expansion connectors. Any idea?
解決済! 解決策の投稿を見る。
Hi, Randa,
From the user manual of LPC55S69, we see that the PLU_IN1 is multiplexed with PIO0_14, which is the node of FC1_I2C_SCL, so the PIO0_14/PLU_IN1 pin is connected to pin11 and pin12 of P19 connector.
Hope it can help you
BR
XiangJun Rong
Hi, Randa,
From the user manual of LPC55S69, we see that the PLU_IN1 is multiplexed with PIO0_14, which is the node of FC1_I2C_SCL, so the PIO0_14/PLU_IN1 pin is connected to pin11 and pin12 of P19 connector.
Hope it can help you
BR
XiangJun Rong
Hello again!
Last time your answer was helpful, I thought maybe this time you can help me to find out how can I trigger the PLU_IN2.
Actually PLU_IN2 is either driven through the pin 8 or pin 80 (see screenshot below)
Now, from the LPC55S69_Board_Shematic_RevA1 we can see that pin 8 is multiplexed with SDO_CARD_DET which can be found on the board in P21 (one of the SD card readers I assume) and U20 (which is a component). While pin 80 is multiplexed with USB1_PortPWR which can be found in U18 (which is a component).
Conclusion: no possibility to drive the PLU_IN2 neither from outside the dev. board nor from within.
Any idea how can I make use of PLU_IN2 ?
Thank you in advance!