LPC4357JBD208E vs LPC4357JBD208K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC4357JBD208E vs LPC4357JBD208K

跳至解决方案
1,446 次查看
amirnat
Contributor I

Hi, what is the difference between LPC4357JBD208E and LPC4357JBD208K ?

I searched in some distributors like Mouser and Digikey, they suggest to buy LPC4357JBD208K instead of LPC4357JBD208E, why? Is there any failure  or other issue? 

I have created a C project for LPC4357JBD208E, can I run it on LPC4357JBD208K

Are LPC4357JBD208E and LPC4357JBD208K pin compatible? can I solder LPC4357JBD208K instead of LPC4357JBD208E?

thank you in advance.

 

0 项奖励
回复
1 解答
1,425 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,436 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

The LPC4357JBD208E package contains 36 PCS, but the LPC4357JBD208K package contains 180 PCS.

LPC4357JBD208E

Active

 

LPC4357JBD208K

Active

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复
1,431 次查看
amirnat
Contributor I

Thank you dear  xiangjun_rong,

Can I replace any of them with each other without any software and/or hardware considerations?

0 项奖励
回复
1,426 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

0 项奖励
回复
1,422 次查看
amirnat
Contributor I

Thank you very much.

0 项奖励
回复