Hi, what is the difference between LPC4357JBD208E and LPC4357JBD208K ?
I searched in some distributors like Mouser and Digikey, they suggest to buy LPC4357JBD208K instead of LPC4357JBD208E, why? Is there any failure or other issue?
I have created a C project for LPC4357JBD208E, can I run it on LPC4357JBD208K ?
Are LPC4357JBD208E and LPC4357JBD208K pin compatible? can I solder LPC4357JBD208K instead of LPC4357JBD208E?
thank you in advance.
Solved! Go to Solution.
Hi, Amir,
The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can replace any of them with each other without any software and/or hardware consideration.
BR
XiangJun Rong
Hi,
Pls refer to the link:
The LPC4357JBD208E package contains 36 PCS, but the LPC4357JBD208K package contains 180 PCS.
Active
Active
Hope it can help you
BR
XiangJun Rong
Thank you dear xiangjun_rong,
Can I replace any of them with each other without any software and/or hardware considerations?
Hi, Amir,
The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can replace any of them with each other without any software and/or hardware consideration.
BR
XiangJun Rong
Thank you very much.