LPC1768 Mini Board EVK UART3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 Mini Board EVK UART3

949 Views
shyamshankar
Contributor II

Hi,

I was able to successfully use the UART0 in the LPC1768 Mini Board for sending and receiving back characters via UART0, based on the LPCOpen Examples. Then I tried to use the UART3 that is available in the EVK, but was unsuccessful. I tried it with different baud rates from 9600 to 921600, but still was not able to make it work.

Has anyone else faced the same issue ??

Is there any jumper settings in the evk that is supposed to be set for using the UART3 ? I did not find any in the datasheet or any other relevant documents relating to this.

I am attaching a picture of the EVK herewith. 

Thank You.

Labels (5)
Tags (2)
0 Kudos
Reply
1 Reply

813 Views
brendonslade
NXP TechSupport
NXP TechSupport

Hi Shyam,

please note this isn't a board made by NXP, so we cant help you with this question. Hopefully there is another community member who will see this and can help.

0 Kudos
Reply