LPC驱动1024*768屏幕显示水波纹

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC驱动1024*768屏幕显示水波纹

878 次查看
saidadiao
Contributor I

使用LPC1788的MPU,驱动1024*768的24位TFT屏幕,LCD时钟为19.2M的时候,屏幕显示图像正常,但有水波纹,频闪现象,LCD时钟为32M的时候,屏幕频闪现象消失,但是出现花屏现象,屏幕撕裂

标签 (1)
0 项奖励
回复
7 回复数

853 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport
0 项奖励
回复

850 次查看
saidadiao
Contributor I
我想知道,LPC1788支持的1024*768分辨率,32位屏的最大LCD时钟频率是多少
0 项奖励
回复

823 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

Are your sure 32 bits? Or 24 bits? 

And do you want to know the max clock source of LPC1788 LCD clock frequency or your LCD frame? 

You can send the datasheet of LCD to me.

 

BR

Alice

0 项奖励
回复

817 次查看
saidadiao
Contributor I
刚回复了屏的规格书,屏颜色深度是24bit的
0 项奖励
回复

740 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @saidadiao 

1) From the DS of LCD you send, the frequency is out of the LPC1788 support:

Alice_Yang_0-1703582184044.png

 

 

2) Please check the configuration of your LCD driver:

HSW HFP HBP VSW VFP VBP

 

BR

Alice

 

 

0 项奖励
回复

719 次查看
saidadiao
Contributor I

谢谢,问题已经解决了

0 项奖励
回复

818 次查看
saidadiao
Contributor I
 
0 项奖励
回复