I want to know some LPCXpresso 54102 - Request of Detail Information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to know some LPCXpresso 54102 - Request of Detail Information

607 Views
rizaltanjung
Contributor I

Hello, I am currently involving in a project which build a power evaluation tool for low-end embedded system. I got a LPCXpresso 54102 board. To do some validation of the power model I built, I want to know some detail information about the core in that board:
1. What is the process technology used for Cortex-M0+ and Cortex-M4 in the MCU (LPC54102)?
2. If I supply 3.3V to VDD on the LPC54102, what is the voltage that on-chip regulator will supply to core? Is it also 3.3V?
I don't know whether that information is confidential or not. If it is not, please give me some help.

Thank you in advanced.

Labels (1)
0 Kudos
Reply
1 Reply

440 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I'm afraid this question has been posted to the wrong forum.  (This forum is about the IDE and debugger.)  You should use the LPC forum at

LPC

Meanwhile this is the kind of detail you may find by starting at

LPC54000|Low Power 32-bit MCUs|Cortex-M4 Core|NXP

Sincerely

LPCXpresso IDE Support

0 Kudos
Reply