Hard fault on OM13098 Rev E (but not Rev C)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard fault on OM13098 Rev E (but not Rev C)

1,428 Views
hugo_gateau
Contributor I

Hi,

We are developing software on OM13092 and we recently try to test it on OM13098 board has there are binary compatible.

I have two OM13098 board on is a rev C and on a rev E (both with a LPC54628).

The same binary works as expected on Rev C but cause a hard fault on Rev E.

We are using FreeRTOS.

I haven't identify what cause the hard fault yet but it is at the very beginning probably during tasks initialization (but after BSP init).

I will continue to investigate but any help would be very appreciated.

Thank you.

Hugo

Labels (2)
Tags (1)
0 Kudos
Reply
7 Replies

1,268 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hugo,

Regarding the difference between COMMAND 0xEB and 0x6B, the SPIFI module just generates the timing based on the command, you have to refer to the data sheet of SPI flash to get the difference.

BR

XiangJun Rong

0 Kudos
Reply

1,268 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hugo,

I think we recommend customer use the spifi driver instead of the libspifi library, the libspifi library is a bit complicated.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

1,268 Views
hugo_gateau
Contributor I

Thank you.

Can you give me more details about the difference between the two commands:

0xEB (Fast Read Quad I/O)

0x6B (Fast Read Quad Output)

As I said we want to be sure about the source of the issue.

0 Kudos
Reply

1,268 Views
hugo_gateau
Contributor I

Thank you for your help,

1)

For now, I integrated the new chip in libspifi by duplicating the configuration used for the W25Q32FV. But I had to change the read command from 0xEB (Fast Read Quad I/O) to 0x6B (Fast Read Quad Output). Using 0xEB we were reading the correct data but in a wrong order (nothing to do with endianess).

The problem is now fixed but I would like to understand the cause of the problem.

2)

I see in your example that the spifi is now integrated in a dedicated driver instead of libspifi.

Do you plan to continue maintaining libspifi and integrated new chips in it ? or is the new recommended way to use only the driver ?

Thank you for your help.

0 Kudos
Reply

1,268 Views
hugo_gateau
Contributor I

After more investigations it happens to be QSPI issue.

We are using LPCSpifilib v1.03 which does not support the new WINBOND QSPI flash (25Q128JVFM).

It causes the memory to fail initialization which leads later to a hard fault.

Is there a version of the LPCSpifilib that support the WINBOND QSPI flash 25Q128JVFM ?

0 Kudos
Reply

1,268 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hugo,

it appears that the spifi driver in SDK package has the W25Q spi flash timing commands.

I attach the code here.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

1,268 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hugo,

You have to track which line of code leads to the hardfault exception.

BR

Xiangjun Rong

0 Kudos
Reply