Flashing issue while using SPIFIDriver_generic demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing issue while using SPIFIDriver_generic demo

1,560 Views
subodhmankar
Contributor II

Hi,
Where does LPC5460x_SPIFI_GENERIC.cfx file gets generated after successful build?

and I am getting following issue while flashing axf file generated by SPIFI_Generic demo

flash_driver_issue.png

Tags (3)
0 Kudos
Reply
1 Reply

1,436 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Subodh Mankar,

Which example projects are you using? The LPC5460x_SPIFI_GENERIC.cfx file is the Flash driver file, it is located in the following folder inside the MCUXpresso IDE installation:

pastedImage_1.png

I would recommend you to check the MCUXpresso SDK examples, you can download the package for the LPC54608 MCUs from this link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

Here is a document on how to generated the SDK package:

https://community.nxp.com/docs/DOC-333304 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer