Clocking of LPC81x SCTimer SCT in UM10601 LPC81x User manual Rev. 1.6 — 2 April 2014

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clocking of LPC81x SCTimer SCT in UM10601 LPC81x User manual Rev. 1.6 — 2 April 2014

507 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by holder@valencell.com on Thu Oct 30 12:40:48 MST 2014
Hi,

Table 121. SCT configuration register (CONFIG, address 0x5000 4000) bit description in the UM10601 LPC81x User manual Rev. 1.6 — 2 April 2014 describes the timer clock options as bus or bus prescaler. Based on Fig 3. LPC81x clock generation it looks like its actually the system clock. I just want to verify this and suggest updating the documentation to reflect that fact...

Best regards,

-Nate
Labels (1)
0 Kudos
Reply
3 Replies

464 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Fri Oct 31 09:48:31 MST 2014
Yes, the SCT clock can be the same speed as the system clock.

Paul
0 Kudos
Reply

464 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by holder@valencell.com on Fri Oct 31 09:25:20 MST 2014
OK, thanks for the info. In that case can the SCT clock can run at the same speed as the system clock?
0 Kudos
Reply

464 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Fri Oct 31 05:42:57 MST 2014
I think that the User Manual is correct.  The prescalers that are referenced in the description are the prescalers built into the SCT.  See the SCT CTRL for details regarding the prescalers.

Paul
0 Kudos
Reply