Can LPC546x's SPIF connect to serial SRAM that supports QSPI?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LPC546x's SPIF connect to serial SRAM that supports QSPI?

668 次查看
geweilin
Contributor II

Since the SPIF can support QSPI interface flash, I wonder this interface can support QSPI SRAM?

标签 (2)
0 项奖励
回复
1 回复

591 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Yes, I think so.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复