Windows10にIDEというタイトルをインストールし、エミュレータ
LPC11U35_QuickStartBoard(Embedded_Artists)としてインストールしました0244_lpc11u35_ssci1114_0x0000.bin上記のファイルを
インストールして、LPC1114FN28用のエミュレータとして
使用します。
使ってみましたが、認識されません。
数年前にWindowsXPにLPCXpresso_6.1.0.164をインストールした状態で、
Debug_Configurations、上記のボードをエミュレータの一種として設定し、
DAP-Linkとして認識した記憶があります。
LPCXpressoに特別な設定が必要ですか?
Hi TakMa
Sorry we can't understand Japanese. Could you please edit your question to English? Thanks a lot.
Have a nice day,
Jun Zhang
About the Emulator in LPCXpresso_v8.2.2.650
I installed the title IDE on Windows10 and as Emulator
LPC11U35_QuickStartBoard(Embedded_Artists),
0244_lpc11u35_ssci1114_0x0000.bin
Install the above file and use it as EmuLator for LPC1114FN28.
I tried using it, but it doesn't recognize it.
With LPCXpresso_6.1.0.164 installed on WindowsXp several years ago,
In Debug_Configurations, set the above board as a type of Emulator,
I remember recognizing it as DAP-Link.
Do I need any special settings for LPCXpresso?
Hi TakMa
This board LPC11U35_QuickStartBoard(Embedded_Artists) is not NXP product and we can't help you test it.
I suggest you checking its usage on the website or with Embedded_Artists support.
https://www.embeddedartists.com/products/lpc11u35-quickstart/
Thanks,
Jun Zhang
We recommended LPC emulator is MCU Link
Thanks,
Jun Zhang