Windows10にIDEというタイトルをインストールし、エミュレータ
LPC11U35_QuickStartBoard(Embedded_Artists)としてインストールしました0244_lpc11u35_ssci1114_0x0000.bin上記のファイルを
インストールして、LPC1114FN28用のエミュレータとして
使用します。
使ってみましたが、認識されません。
数年前にWindowsXPにLPCXpresso_6.1.0.164をインストールした状態で、
Debug_Configurations、上記のボードをエミュレータの一種として設定し、
DAP-Linkとして認識した記憶があります。
LPCXpressoに特別な設定が必要ですか?
I will buy MCU-LINK and see if LPCXpresso recognizes it or not. If there is a problem with my confirmation, please help me again. I'll close this question. Thank you for your support.
Hi TakMa
Sorry we can't understand Japanese. Could you please edit your question to English? Thanks a lot.
Have a nice day,
Jun Zhang
About the Emulator in LPCXpresso_v8.2.2.650
I installed the title IDE on Windows10 and as Emulator
LPC11U35_QuickStartBoard(Embedded_Artists),
0244_lpc11u35_ssci1114_0x0000.bin
Install the above file and use it as EmuLator for LPC1114FN28.
I tried using it, but it doesn't recognize it.
With LPCXpresso_6.1.0.164 installed on WindowsXp several years ago,
In Debug_Configurations, set the above board as a type of Emulator,
I remember recognizing it as DAP-Link.
Do I need any special settings for LPCXpresso?
Hi TakMa
This board LPC11U35_QuickStartBoard(Embedded_Artists) is not NXP product and we can't help you test it.
I suggest you checking its usage on the website or with Embedded_Artists support.
https://www.embeddedartists.com/products/lpc11u35-quickstart/
Thanks,
Jun Zhang
Now, as the Emulator in LPCXpresso_v8.2.2.650
Please tell me which boards are available.
We recommended LPC emulator is MCU Link
Thanks,
Jun Zhang