關於LPC1850 ADC 電壓範圍限制問題?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

關於LPC1850 ADC 電壓範圍限制問題?

625 次查看
ericliao
Contributor I

硬體線路說明:

(1) LPC1850應USB self-power device

(2) ADC0_2(A4 pin)經由R103及R104  10K分壓電阻去偵測USB0_VBUS電壓的狀況

ADC0_2.jpg

問題  : 由於是USB self-power供電 ,會有USB0_VBUS有電MCU未供電的情況發生

此時是否會造成ADC0_2 pin(<3.6V)的損害?

依照Datasheet描述:

(a) 使用ADC0_2設定在 5V Tolerant pad(ex:PF_8)是可接受<3.6V

ADC1.jpg

ADC2.jpg

(b) 使用ADC0_2 (A4 pin)單獨在analog pad並未說明是否承受3.6V以下電壓

ADC3.jpg

ADC4.jpg

Thanks

Eric @SAC

0 项奖励
回复
1 回复

564 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Eric,

After contacted with the AE, they'd like to suggest the the analog input doesn't exceed the 3.6V.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------