有关LPC1769芯片原理图与PCB文件下载

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

有关LPC1769芯片原理图与PCB文件下载

1,404 次查看
jiangjian1208
Contributor I

有关LPC1769芯片原理图与PCB文件下载

标签 (1)
0 项奖励
回复
4 回复数

1,281 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello an jian,

I just was wondering which board ?

For example LPCXpresso board for LPC1769, you can download schematic on NXP website:

LPCXpresso board for LPC1769 with CMSIS DAP probe|NXP 

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,280 次查看
jiangjian1208
Contributor I

您好:

是这样的,我要用Altium Designer软件画工程电路设计图。我需要贵公司支持的芯片图,与封装文件,我记得以前在公司的网站上可以下载的,为什么现在下载不到呢。这样我就不用自己画芯片的原理图引脚了

发送自 Windows 10 版邮件<https://go.microsoft.com/fwlink/?LinkId=550986>应用

0 项奖励
回复

1,280 次查看
jiangjian1208
Contributor I

I need to use atium designer to design the circuit diagram and lpc1769 chip. Now I need the schematic diagram and pin diagram of the chip and the PCB package engineering library file.I don't know if you can understand me

0 项奖励
回复

1,280 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello an jian,

There is only the LIB for ORCAD, no Altium Designer.

LPC1769FBD100|Arm Cortex-M3|32-bit MCU|NXP 

pastedImage_1.png

Maybe you can try to  search , whether there is a method to  convert it to  Altium Designer Lib.

BR

Alice

0 项奖励
回复