K22 I2C SDK Driver behaving strangely? (As in failing...)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22 I2C SDK Driver behaving strangely? (As in failing...)

Jump to solution
4,526 Views
bosleymusic_com
Contributor IV

EDIT (The Short Story) : IICIE does not set after  I2C_HAL_SetIntCmd(baseAddr, true); in I2C_DRV_MasterSendDataBlocking, but it does set and goes through its proper courses when used in I2C_DRV_MasterReceiveDataBlocking. So, 0x04 timeouts on sends, 0x00 successful receives, but using the exact same subfunction to enable the interrupt? Makes no sense unless there is some other bit combination it isn't compatible with....If I manually set IICIE after the I2C_HAL_SetIntCmd(baseAddr, true); in I2C_DRV_MasterSendDataBlocking, transmission succeeds, so I know the bit needs to be set manually somehow...will update on that.

 

The Long Story:

Currently trying to program registers of a Max 98090 Audio CODEC. Works perfectly with another device, but running into some static with my K22 FRDM board using the Master Driver.

This version of Max98090 addresses at 0x20 / 0x21 for W/R, so my address variable is set at 0x10 (0010000). hardware seems to be initialized properly and based on scope/timings is operating "properly."

I had the I2C comm demo working and have tried to copy as many of my settings as possible from that.

 

Variations I have tried:

I have tried using I2C1 on different pins, and noticed it helped square off my waveforms, likely because it isn't sharing any leads/trace with another device as I2C0 on PB2/3 is (hooked to the accel/mag).

No pullups, 1k, 2.2k, and 10k. No major differences. Tried 50, 100, 400kHz. 50 kHz times out, but 100 and 400 work.

 

Using Master Send Data results in the correct address, and ACK from the CODEC as slave, but nothing beyond that....returns time out every time. If I stop the transfer with a breakpoint and manually set the IE before the send address bit it works, otherwise no dice. (The interrupts work for master receive)

16270_16270.pngNoACK.png

 

Master Receive is successful, but works strangely compared to my previous experience with I2C and TWI. In order to read one byte, it goes through the following sequence :

1)Start, send address (Write address, not read?)

2)Sends the Register value I want to read

3)Sends a read address

4) Reads the actual value (correctly)

16271_16271.pngWrite.png

Why start out with a write instead of starting with a read address directly, followed by the register, and then receive a value? Is there a specific reason in logic, performance, or mechanics?

Labels (1)
Tags (3)
1 Solution
3,209 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Donald:

Your code seems ok to me.

I did a quick test with KDS v.1.1.1 and FRDM-K22F calling the MasterSendDataBlocking() function and the interrupt triggers just fine.

Can you try removing the call to MasterReceive function? I mean calling just MasterSend, and see if the issue persists.

I am curious about how are you reading the IICIE bit. Did you install the registers view plugin for KDS?

If you already identified that the API I2C_HAL_SetIntCmd is the problem, then it might be related to the compiler (optimizations maybe). In debug mode you have the Disassembly view, so I would compare the code generated for this API when calling MasterReceive vs MasterSend.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
9 Replies
3,209 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Donald:

- What pins are you using? In the file pin_mux.c you will find a function called "pin_mux_I2C()". The pins you use need to be configured as open-drain and also external pull-ups are necessary.

- Repeated start errata is not present in K22FN512.

- How are you using the API's? Can you show a code snippet vs the codec protocol?

- As you mentioned, both driver functions use the same HAL API to enable interrupts, so it might be strange if this is the problem. Besides we have used the I2C Driver without issues, check this: KSDK I2C EEPROM Example.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,209 Views
bosleymusic_com
Contributor IV

I have looked at the i2c_comm master example and had it working with uc_iii to send between I2C0 and 1 on the same board. Right now I'm running this in BM_OS. Will look at the EEPROM example.


Definitely have the open drains enabled in my pin-setup:

/***** I2C PINS *****/

  /*  I2C0 */

  /* PORTB_PCR2 - CLOCK */

  PORT_HAL_SetMuxMode(g_portBaseAddr[1], 2u, kPortMuxAlt2);

  PORT_HAL_SetOpenDrainCmd(g_portBaseAddr[1], 2u, true);

  /* PORTB_PCR3 - DATA */

  PORT_HAL_SetMuxMode(g_portBaseAddr[1], 3u, kPortMuxAlt2);

  PORT_HAL_SetOpenDrainCmd(g_portBaseAddr[1], 3u, true);

External pull-ups are used. Right now they are 10k's, but I have tried two other values (1k, 2.2k) with the same results in terms of RX working, TX not.

Declared locally to the function :

/***** I2C VARS *****/

  i2c_master_state_t i2c0_master_state;

  i2c_status_t i2c_status;

  i2c_device_t

  i2c0_codec =

  {

  .address = 0x10, (Actually 0x20 and 0x21)

  .baudRate_kbps = 400

  };

  /*****  I2C TX/RX VARIABLES *****/

  uint8_t cmdbuff[1];

  uint8_t txbuff[1];

  uint8_t rxbuff[1];

Init:

/****** INITIALIZE I2C ******/

  I2C_DRV_MasterInit(0, &i2c0_master_state);

/***** TEST REMOVE AFTERWARDS *****/

  cmdbuff[0] = 0x26;

  rxbuff[0] = 0;

  i2c_status = I2C_DRV_MasterReceiveDataBlocking(0, &i2c0_codec, cmdbuff,

  sizeof(cmdbuff), rxbuff, sizeof(rxbuff), 500);

^ THIS SETS rxbuff[0] TO 0x80 WHICH IS THE VALUE OF 0x26 in the codec after Reset... good to go

cmdbuff[0] = 0x26;

  txbuff[0] = (0 | (1 << 6));

  i2c_status = I2C_DRV_MasterSendDataBlocking(0, &i2c0_codec, cmdbuff,

  sizeof(cmdbuff), txbuff, sizeof(txbuff), 500);

^ THIS SENDS THE ADDRESS, SLAVE ACKS, however the function that should set IICIE does not set that bit (bit 6), so it doesn't go through the ISR after HAL Send Start, producing 0x04 time out for the status.

------

I had the cmdbuff, tx and rxbuff set as pointers, but I was getting compiler errors for passing arguments of incompatible type, which makes sense I think because a declaration of an array is already a pointer. Other than that, I'm stupmed, and thank you for the quick response.

0 Kudos
Reply
3,210 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Donald:

Your code seems ok to me.

I did a quick test with KDS v.1.1.1 and FRDM-K22F calling the MasterSendDataBlocking() function and the interrupt triggers just fine.

Can you try removing the call to MasterReceive function? I mean calling just MasterSend, and see if the issue persists.

I am curious about how are you reading the IICIE bit. Did you install the registers view plugin for KDS?

If you already identified that the API I2C_HAL_SetIntCmd is the problem, then it might be related to the compiler (optimizations maybe). In debug mode you have the Disassembly view, so I would compare the code generated for this API when calling MasterReceive vs MasterSend.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,209 Views
bosleymusic_com
Contributor IV

Look at the assembly...bingo! Maybe....?

The question is, how do I change it?

RECEIVE:

413           I2C_HAL_SetDirMode(baseAddr, kI2CSend);

0000157c:   ldr r0, [r7, #24]

0000157e:   movs r1, #1

00001580:   bl 0xe70 <I2C_HAL_SetDirMode>

416           I2C_HAL_ClearInt(baseAddr);

00001584:   ldr r0, [r7, #24]

00001586:   bl 0xf88 <I2C_HAL_ClearInt>

417           I2C_HAL_SetIntCmd(baseAddr, true);

0000158a:   ldr r0, [r7, #24]

0000158c:   movs r1, #1

0000158e:   bl 0xf60 <I2C_HAL_SetIntCmd>

SEND:

323           I2C_HAL_SetDirMode(baseAddr, kI2CSend);

0000143c:   ldr r0, [r7, #24]

0000143e:   movs r1, #1

00001440:   bl 0xe70 <I2C_HAL_SetDirMode>

326           I2C_HAL_ClearInt(baseAddr);

00001444:   ldr r0, [r7, #24]

00001446:   bl 0xf88 <I2C_HAL_ClearInt>

328    

0000144a:   ldr r0, [r7, #24]

0000144c:   movs r1, #0

0000144e:   bl 0xf60 <I2C_HAL_SetIntCmd>

331           I2C_HAL_SendStart(baseAddr);

00001452:   ldr r0, [r7, #24]

00001454:   bl 0x25e8 <I2C_HAL_SendStart>

0 Kudos
Reply
3,209 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Donald:

Yes, that must be the problem. This is what I get:

pastedImage_0.png

This code is part of the platform library, so you should look there instead of your application. Do you remember changing any project setting of the K22 KSDK library (e.g. optimizations)?

Also, notice that in my case the MasterSend() code calls the API at line 327, while in your case it is missing.

Regards!

Jorge Gonzalez

3,209 Views
bosleymusic_com
Contributor IV

I rebuilt the library and the i2c master driver c file showed up as modified upon rebuild. Everything is working now. Thank you.

3,209 Views
bosleymusic_com
Contributor IV

Thank you for verifying. I haven't changed anything in terms of the lib.a or associated files.

Do you think rebuilding the library could potentially solve this?

I'm not super saavvy when it comes to toolchains and compiler mechanics, so if you could offer some suggestions as to what to look for or how to approach the error, I can probably hunt it down for a fix.

0 Kudos
Reply
3,209 Views
bosleymusic_com
Contributor IV

- I am using the EmbSys plug-in to do register reads (another Eclipse on MCU tutorial), and that's how I was able to set the IICEN bit.

- I just built a test function with only the bare essentials running, but same issue - I will upload an exported archive if you get a chance to check it.

- Commented out Master Receive. Send still doesn't work on its own, but returns 0x00 for manually setting the IICEN bit by using a breakpoint before Send Start.

- Will check dis-assembly view, although I'm not much of an assembly guy so I'll probably end up posting it here.

0 Kudos
Reply
3,209 Views
bosleymusic_com
Contributor IV

Maybe something to do with this? Re: Kinetis K - I2C: Repeat start cannot be generated?

0 Kudos
Reply