Is there any tool like PE in SDK 2.0???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any tool like PE in SDK 2.0???

624 Views
sywksmstkadlfgk
Contributor III

I have used PE with SDK 1.3 with KDS 3.0, so that it is easy to add the component to the project and configure the pins and initiate the component, let me to focus the program of application. And now there is KDS 3.2 and SDK 2.0, but there is not PE support. I need to study the datasheet and understand the registers on the component to initiate the pinmux and set the registers.

 

Is there any tool like PE in SDK 2.0  to make program easy?

 

Thanks.

 

Zhong Shen,,

Labels (1)
0 Kudos
Reply
1 Reply

422 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Zhong Shen,

I am sorry, but ksdk 2.0 does not have Processor Expert support available.  A new suite of configuration tools is being created that will build on KSDK v2 and will be rolled out throughout 2016.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply