"MCU-Link Debug Probe" to be used with "Keil MDK IDE" and "NXP MCUXpresso IDE"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"MCU-Link Debug Probe" to be used with "Keil MDK IDE" and "NXP MCUXpresso IDE"

1,911 Views
hfabbasi
Contributor III

I have designed a board using "NXP MK60DX256" micrcontroller where I used "TWRK60D100M" kit's pin configuration for JTAG as shown in "picture 1"  (namely "Coretx Debug 10-Pin Connector" topology as shown in "picture 2")  for downloading program and debugging purpose.  I coded my program in "Keil MDK IDE" and succesfully used "Keil ULINKpro" debugger for downloading program. Now I want to shift to "NXP MCUXpresso IDE" for writing my code. I purchased "NXP MCU-Link Debug Probe" which have debug connector as shown in "picture 3". When I use "MCU-Link Debug Probe" with  "Keil MDK IDE", I am able to download my program. But I am unable to download my program using  "NXP MCUXpresso IDE" as shown in picture 4 and 5 because "0 available SWD devices detected" error comes up. For the record to make picture 1 compatible with picture 3, I have removed pin 7 from "MCU-Link debug probe" and left pin 9 of  "MCU-Link debug probe"  floating.

0 Kudos
Reply
1 Reply

1,892 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

How did you power the TWR-K60D100M board? 
When power TWR-K60D100M board by J17, I am able to debug board with MCU-Link Debug Probe.
No need to left pin 9 of "MCU-Link debug probe" floating, the pin 9 of J16 on TWR-K60D100M is not connect to other signal.(DNP)
No need to removed pin 7 of "MCU-Link debug probe", the pin 7 of J16 on TWR-K60D100M is not connect to other signal too.

Probes discovered.pngMCU-LINK TWR-K60D100M.jpg

I am using MCUXpresso IDE v11.4.1 [Build 6260] [2021-09-15].


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply