Kinetis Device is Locked. Do you want to unlock it? Mass erase will be executed. MK60DX256VLL10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Device is Locked. Do you want to unlock it? Mass erase will be executed. MK60DX256VLL10

3,901件の閲覧回数
hfabbasi
Contributor III

I am using MK60DX256VLL10 in a circuit. After soldering the controller onto the designed board, I tried to download my code into the controller using Ulink Pro Debugger using Keil MDK. But i encounter "Kinetis Device is Locked. Do you want to unlock it? Mass erase will be executed" to which I press OK. After few seconds, "Invalid ROM table" appears and erase is not performed. 

To be cear, the same code is used in another board where same controller is used and in that board, I am able to doanload my code wihtout any "lock isssue" or "invalid rom table" issue.

0 件の賞賛
返信
3 返答(返信)

3,881件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @hfabbasi ,

Maybe the chip isn't really locked. There is some soldering issue or hardware problem. Please refer to this guide.

 

Regards,

Jing

0 件の賞賛
返信

3,862件の閲覧回数
hfabbasi
Contributor III

Your suggested document is very thorough. It really helped me to understand the problem I am facing. Regarding unlocking the chip, I want your help in unlocking my device. I have "Keil ULINKpro" debugger hardware which I am using with "Keil MDK IDE" or "NXP MCUXpresso IDE" software. I dont have "J Link/ FLasher" hardware which is being in your suggested pdf document. So, how "Keil ULINKpro" debugger hardware can be used with "Keil MDK IDE" or "NXP MCUXpresso IDE" software to unlock my device? 

0 件の賞賛
返信

3,842件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @hfabbasi ,

Please refer to this link.

https://developer.arm.com/documentation/ka003053/latest

But if the problem is caused by hardware or other issue, it won't help.

 

Regards,

Jing

 

0 件の賞賛
返信