:smileyhappy:
Hi
Today, I use TWR-K65F180M board do a test using KSDK V1.2 provides mfs example (located at C:\Freescale\KSDK_1.2.0\middleware\filesystem\mfs\examples\sdcard).
Below is the test hardware:
During my test, I find the mfs does support to create the folder with . prefix.
Below video shows the detailed test info (sorry for my input error command, I should input "type 3.txt" instead, which extend the video time).
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
It is possible that the file system that you are using doesn't (correctly) support long file name (LFN).
See chapter 13 of http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF for details of LFN operation.
There is also a possibility that the handling is an option that needs to be enabled in the FAT library.
Regards
Mark
Kinetis: µTasker Kinetis support
utFAT2.0: http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF
For the complete "out-of-the-box" Kinetis experience and faster time to market