I recently bought the HVP-KV46F150M kit to run a BLDC motor. I used Kinetis Design Studio 3.2.0 to build the demo file mc_bldc_hvpkv46f150m and download to the microcontroller. Followed the HVP-KV46F150M Quick Start Guide to test the motor. I connected a 750W BLDC motor and when I power up, it runs a few truns and stops as there is no load connected to it.
The issue I am having is that I am unable to monitor the project with FreeMaster 3.1. I used PMSM_Sensorless_FOC.pmp file and when I click on the GO button I am getting this error
From KDS I am able to connect to the board with the same com port, so I know the com driver is working. Please help to get the FreeMaster 3.1 to monitor and control the BLDC motor.
Solved! Go to Solution.
MCUXpresso SDK and IDE are recommend.(KDS is too old)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
MCUXpresso SDK and IDE are recommend.(KDS is too old)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------