USB Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Bootloader

3,293 Views
kp2309
Contributor I

Hi Guys,

 

We are using K60 series. Looking for a USB bootloader. If it is inbuilt, will it take care of USB driver as well or we have to drive the usb by some other means (OS or driver if we have access to bootloader source)?

If we need other OS to drive USB then is it worth to use a seperate OS just to drive USB or there is any other method where we can use USB bootloader for firmware upgradation?

If there is no inbuilt USB bootloader from where can I get it?

 

Please share your suggestions.

 

-KP

0 Kudos
Reply
3 Replies

2,816 Views
dhaval_v_shah
Contributor III

Hi KP,

 

USB bootloader is not built in.

 

You will need USB driver to driver the USB, for that you can use OS with support for USB, infact if you go for OS with USB booloader support you will get USB driver built in.

 

Regards,

Dhaval

0 Kudos
Reply

2,816 Views
dhaval_v_shah
Contributor III

Hi KP,

 

There is application note for USB bootloader under

"Freescale.com>products>kinetis>K60>Documentation>Application notes" for USB boot loader.. The application note explains bare metal and MQX based USB Bootloader.

 

Regards,

d2v0!

0 Kudos
Reply

2,816 Views
mjbcswitzerland
Specialist V

Hi

 

See:

- http://www.youtube.com/watch?v=H4TYM9jY2-g (showing K60 tower kit)

- http://www.youtube.com/watch?v=e4oFBn_M5wo (shown on another chip but also works on Kinetis)

 

- http://www.youtube.com/watch?v=nm2DmZv1rj8&feature=related (shown for K40 modules but emphasis on SLCDs)

 

 

Regards

 

Mark

 

 

0 Kudos
Reply