SRAM size and location for MK64FX512VLL12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRAM size and location for MK64FX512VLL12

ソリューションへジャンプ
1,104件の閲覧回数
steve32768
Contributor II

Can someone from NXP please confirm the SRAM size and address range for the MK64FX512VLL12?

Per the datasheet, this should be 256KB, but there's conflicting information in the reference manual. The reference manual indicates a size of 256 KB, but address range of 0x1FFF_0000-0x2001_FFFF (which is only 192 KB)

See attached picture from the table in section 3.5.3.1 of the latest reference manual v.5. 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,087件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.

元の投稿で解決策を見る

3 返答(返信)
1,083件の閲覧回数
steve32768
Contributor II

Thanks for the quick reply on that!

0 件の賞賛
返信
1,094件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, the MK64FX512VLL12 has 256 KB of SRAM. Still, I will escalate your remarks on the address ranges in the Reference Manual as a possible documentation error and will get back to you as soon as I receive a response.

 

Regards,

Edwin.

1,088件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Interal concurred with the documentation error. The address ranges of all the listed devices should be 0x1FFF_0000 - 0x2002_FFFF. Thanks for reporting this mistake.