Over-the-Air Firmware Update in MKW36A512?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Over-the-Air Firmware Update in MKW36A512?

ソリューションへジャンプ
1,066件の閲覧回数
ajith_k
Contributor I

Hi,

We would like to use MKW36A512 SoC in one of our new designs. OTA update is a feature that we require in the design. Does Kinetis MKW36A512 support OTA firmware update?

Expecting a quick resolution.

Thanks and regards

ラベル(1)
0 件の賞賛
返信
1 解決策
976件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Ajith, I hope you're doing well!

 

The BLE Stack developed for the KW36 family of MCUs has support for OTAP, and there's currently an example implementing a simple OTA Client Application included in the SDK package for this device.

 

The MCUXpresso SDK builder can be used for building and downloading the SDK for the KW36Z/A.

 

The OTAP Client example can be found in the following path of the SDK:

<…\SDK_2.2.2_FRDM-KW36\boards\frdmkw36\wireless_examples\bluetooth\otac_att>

 

And information about running the example can be found in the BLE Demo Applications User's Guide:

<…\SDK_2.2.2_FRDM-KW36\docs\wireless\Bluetooth\Bluetooth Low Energy Demo Applications User Guide.pdf>

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
977件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Ajith, I hope you're doing well!

 

The BLE Stack developed for the KW36 family of MCUs has support for OTAP, and there's currently an example implementing a simple OTA Client Application included in the SDK package for this device.

 

The MCUXpresso SDK builder can be used for building and downloading the SDK for the KW36Z/A.

 

The OTAP Client example can be found in the following path of the SDK:

<…\SDK_2.2.2_FRDM-KW36\boards\frdmkw36\wireless_examples\bluetooth\otac_att>

 

And information about running the example can be found in the BLE Demo Applications User's Guide:

<…\SDK_2.2.2_FRDM-KW36\docs\wireless\Bluetooth\Bluetooth Low Energy Demo Applications User Guide.pdf>

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信