OpenOCD with FRDM-K64F support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenOCD with FRDM-K64F support

3,958 次查看
stanymarcel
Contributor I

Hi,

I'd like to debug my FRDM-K64 with OpenOCD. I built it with cmsis-dap support from the master of openocd git.

I tried to make it work by adapting the k60.cfg with cortex_m4 chip ID, but I can't get it work properly (not supported MCU error when i try to attach gdb) .

Is there somewhere some patch or special tcl config for k64 available ?

What version of OpenOCD is used in KDS (waiting for download approval) ?

Are the tcl used by KDS available somewhere (kinetis.cfg and k64.cfg)

Regards

0 项奖励
回复
1 回复

1,548 次查看
BlackNight
NXP Employee
NXP Employee

By now you should have received the download link, otherwise let me know.

The scripts/tcl files are located inside C:\Freescale\KDS_1.0.1\openocd\scripts (attached)

Regards,

Erich

0 项奖励
回复