Dear Kinetis-Team,
i have a complain about the Kinetis MCUs, K22FN512.
I did all the art for a good adc result:
1. Voltages are highly stable and noise free
2. ADC inputs are driven by ADC-Driving OpAmps
3. Reference voltage is stable.
4. Solid GND Plane
However, I get noise on my result:
Its 12 binary digits noise at 12 Bit conversion. Thats too much for me, as I want to use the adc in a control loop.
Its approx 0,2%-0,3% noise in the measurement range but this is too much for a good adc, like the datasheet promises.
What can I do better to improve my performance? I want to switch to Kinetis KV44. Will there be better results?
I'm pretty sure you won't do a new revision, but please make more sure next time, you get a good and stable adc result.
Other people also complained with similar results.
https://community.nxp.com/thread/322988
解決済! 解決策の投稿を見る。
Hi,
thanks Ma Hui for your support. I checked that I followed all the recommended steps.
What I tried and did not help:
Current state: 0.15% noise
Practically, I have the same problem as you describe in the 19 counts off example.
-Replaced switching regulator with lab power supply. Same issue.
-Vss&Vref are already highly bypassed.
-No chance to place ferrite beads in the design. However, as no more switching device is left, nor any noise can be seen with 12 bit oscilloscope, i guess this will not make a difference.
-played with sample time: No difference. ADC Channels are actively driven by opamp, so i guess this won't be an issue anyhow.
-reduce the clk divder highly. Same issue.
What helped (if you have same problem):
Changed clk source from Bus Clk to Oscillator Clock: OSCERCLK
So I recommend using OSCERCLK with 8MHz.
Now i have 0.07% noise, which meets the Freescale minimum spec of 10.4 effective bits.
How to calulate: 1/2^ENOB=0,074%
What I guess (it's just a guess, based on the made experience): The Busclock is not stable enough, has some gitter? I use standard 120MHz option for KN512. When I change the frequency from 10MHz to 5MHz same issue.
In case everything else fails:
Oversampleing and averaging.
Generally I would like to have a more stable adc.
Update: The KE1xF seems to have an decent ADC. Guess, I will use that part.
Hi
There with some suggestions about how to get better performance of Kinetis SAR ADC:
[ADC Calibration]
[Hardware Configuration]
[ADC Configuration]
There also with an application note AN4373 about SAR ADC cookbook, please check here for the detailed info.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
thanks Ma Hui for your support. I checked that I followed all the recommended steps.
What I tried and did not help:
Current state: 0.15% noise
Practically, I have the same problem as you describe in the 19 counts off example.
-Replaced switching regulator with lab power supply. Same issue.
-Vss&Vref are already highly bypassed.
-No chance to place ferrite beads in the design. However, as no more switching device is left, nor any noise can be seen with 12 bit oscilloscope, i guess this will not make a difference.
-played with sample time: No difference. ADC Channels are actively driven by opamp, so i guess this won't be an issue anyhow.
-reduce the clk divder highly. Same issue.
What helped (if you have same problem):
Changed clk source from Bus Clk to Oscillator Clock: OSCERCLK
So I recommend using OSCERCLK with 8MHz.
Now i have 0.07% noise, which meets the Freescale minimum spec of 10.4 effective bits.
How to calulate: 1/2^ENOB=0,074%
What I guess (it's just a guess, based on the made experience): The Busclock is not stable enough, has some gitter? I use standard 120MHz option for KN512. When I change the frequency from 10MHz to 5MHz same issue.
In case everything else fails:
Oversampleing and averaging.
Generally I would like to have a more stable adc.
Just checked with the datasheets: The ADC of the Kinetis just seems so bad, as i measured.
If you look at STM parts, eg. STM32F334, they have a 10dB better SNR ADC build in. I strongly recommend to improve the ADC on the Kinetis devices.
The KV4x 4MSPS ADC gets even worse: It has 9.1 effective bits. Oversampling by a factor of 4 increases the effective bits by 1. This means that that ADC is useless in the KV4x. I need a better ADC on the KVx series!
The KV5 ADC is better, but I cannot afford double the price...