hi,
I need to flash"Kinetis K22F MCU flash *.efl file without projct" in the factory side.
#Solution 1, "Flash from file..." in KDS, but don't work if without project. You know, we don't want to open code to the factory side.
#Solution 2, If there is a CMD option in KDS, to transfer *.elf to *.hex file or generate *.hex file. and then I can use J-flash SW tool to flash the chip.
Best regards,
Kent
解決済! 解決策の投稿を見る。
Hello Kent,
For your solution 1 : You needn't open your project , you can utilize the any simple project when flash ,
only need choose the .elf file you want to flash , as this :
pay attention , configure correctly of the debugger , for example , if use the J-link , configure the correct "Device name"
About your solution 2: The KDS can directly generate the ".hex" file, you can refer to here :
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kent,
For your solution 1 : You needn't open your project , you can utilize the any simple project when flash ,
only need choose the .elf file you want to flash , as this :
pay attention , configure correctly of the debugger , for example , if use the J-link , configure the correct "Device name"
About your solution 2: The KDS can directly generate the ".hex" file, you can refer to here :
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------