I use KSDK 1.1.0 and KDS 2.0, After i create a Kintetis Design Studio project, I select a MQX_KSDK compoents library to add to project, after i change osa1:fsl_os_abstraction OS name from BareMetal to the MQX_KSDK, mqx_ksdk:MQX_KSDK components have a error "Component name conflicts with another source code module name. (Component name) mqx_ksdk/Component name | Processor Expert Problem" |
,i do not know how to To solve this problem
解決済! 解決策の投稿を見る。
Hi Junfeng,
When use MQX_KSDK, it needn't add the mqx_ksdk component, we only need choose here :
this function is equivalent to MQX_KSDK. There are all the OS the KSDK concluded, we can refer to our need select.
And I test only use the mqx_ksdk component, it show this error below :
So, please do as i said.
Another point, if there are more than one clock under "Clock configuration", please click the "-" to only one.
like this :
Best Regards,
Alice
------------------------------------------------------------------------------------------
If this post answers your question, please click the Correct Answer button.
-----------------------------------------------------------------------------------
If this post help your question, please click the helpful Answer button.
Hi Junfeng,
Do you mean change here :
can you show your screenshot about your configration , or it is difficult find your problem.
Best Regards
Alice
All picture is in the attachment
Best regards
王俊峰 wang junfeng
***************************************************
南京大全自动化科技有限公司little
南京大全自动化科技有限公司 NANJING DAQO AUTOMATION TECHNOLOGY CO., LTD.
江苏省南京市江宁区隐龙路28号 NO.28.Yinlong Road,Jiangning,Nanjing,Jiangsu P.R. China 211100
TEL: (86)025-66987659 (86)13813041588
FAX: (+86)025-66987659
E-mail: wangjunfeng@daqo.com web: <http://www.daqo.com/> www.daqo.com
***************************************************
发件人: Alice_Yang
发送时间: 2014年12月19日 10:33
收件人: 俊峰 王
主题: Re: - KSDK 1.1.0 and KDS 2.0
<https://community.freescale.com/> Freescale Community
KSDK 1.1.0 and KDS 2.0
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/464150?et=watches.email.thread#464150>
Hi Feng,
From your screenshot error :
I think there two fsl_os_abstraction, you can expand thte "Referenced_Components" , see where is error ?
When you create the project , there have fsl_os_abstraction component . Do you need two fsl_os_abstraction component ?
Below attachment is on my side test , if you want, you can send the error project to me .
Best Regards
Alice
error project is in attachment
wjffsx
发件人: Alice_Yang
发送时间: 2014年12月19日 16:12
收件人: 俊峰 王
主题: Re: - KSDK 1.1.0 and KDS 2.0
<https://community.freescale.com/> Freescale Community
KSDK 1.1.0 and KDS 2.0
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/464267?et=watches.email.thread#464267>
Hi Feng,
I have check you project, and many place you haven't configration, for example :
and else.
Use the PE, you can configration refer to its error.
And the attachment is a simple code , and it can work on my side , you can try it ,if ok, you can go on you application on it.
Hope it helps
Alice
See the attachment picture,all is create by PE,is it correct?
Wang junfeng
发件人: Alice_Yang
发送时间: 2014年12月19日 20:50
收件人: 俊峰 王
主题: Re: - KSDK 1.1.0 and KDS 2.0
<https://community.freescale.com/> Freescale Community
KSDK 1.1.0 and KDS 2.0
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/464374?et=watches.email.thread#464374>
Hi Junfeng,
When use MQX_KSDK, it needn't add the mqx_ksdk component, we only need choose here :
this function is equivalent to MQX_KSDK. There are all the OS the KSDK concluded, we can refer to our need select.
And I test only use the mqx_ksdk component, it show this error below :
So, please do as i said.
Another point, if there are more than one clock under "Clock configuration", please click the "-" to only one.
like this :
Best Regards,
Alice
------------------------------------------------------------------------------------------
If this post answers your question, please click the Correct Answer button.
-----------------------------------------------------------------------------------
If this post help your question, please click the helpful Answer button.
Hi Alice,
I did the exact same as you suggested. But, when I do debugging, I get the error ("assertion "!status" failed: file "../SDK/rtos/mqx/mqx/sou") on HyperTerminal.
Do you have any idea how to fix it?
Thanks,
Christie
Hi Alice,
Did you find any problem on my project? If so, please let me know how to fix the problem?
Thanks,
Christie
Hi,
I reinstall KSDK 1.1.0 and KDS 2.0, checking update in KDS, delete workspace , recreate new project, error still there.
I find your picture diff with me ,it is same version ?
the attachment have simple new project code.
wang junfeng
发件人: Alice_Yang
发送时间: 2014年12月19日 20:50
收件人: 俊峰 王
主题: Re: - KSDK 1.1.0 and KDS 2.0
<https://community.freescale.com/> Freescale Community
KSDK 1.1.0 and KDS 2.0
reply from Alice_Yang <https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/464374?et=watches.email.thread#464374>