In the K12 Sub Family reference manual, document # K12P80M50SF4RM, there is Table 42-41, which is the I2C Divider and Hold Values table. Is there a diagram anywhere that shows what the SDA Hold Value and the SCL Hold Start/Stop Values are?
Also, it says those values are in 'Clocks', so does that mean that if I am running at 8Mhz, then the SCL Hold Value for the first entry in that table would be 7/8000000, or 875 nanoseconds? It is just unclear to me, so any info will be much appreciated. Thank you
解決済! 解決策の投稿を見る。
Please related the SDA hold time, the SCL start hold time, and the SCL stop hold time interpretation at I2C Frequency Divider register (I2Cx_F) [ICF] bit description.
It located at page983 of K12P80M50SF4RM.
It also provides an example.
Wish it helps.
Best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Ma! This does solve the question.
Please related the SDA hold time, the SCL start hold time, and the SCL stop hold time interpretation at I2C Frequency Divider register (I2Cx_F) [ICF] bit description.
It located at page983 of K12P80M50SF4RM.
It also provides an example.
Wish it helps.
Best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------