Hi.
I'd like to measure a current by S.E. SAR ADC without shunt resistance.
I connect a sensor output to ADC direct. This sensor output sensing data by current.
Could you give me an idea for above function.
Best regards,
M.Kiniwa
解決済! 解決策の投稿を見る。
Hi, Masahiro,
I think your question is which sensor can be used to convert the current to voltage except shunt resistor. As Earl said, you can use the following sensor to convert current to voltage:
Hall sensor, Rogowski coil sensor, shunt resistor. If you test AC current, you can use current transformer.
Hope it can help you
BR
xiangjun Rong
Hi, Masahiro,
I think your question is which sensor can be used to convert the current to voltage except shunt resistor. As Earl said, you can use the following sensor to convert current to voltage:
Hall sensor, Rogowski coil sensor, shunt resistor. If you test AC current, you can use current transformer.
Hope it can help you
BR
xiangjun Rong
Hi EARL, Xiangjun
Thank you for your reply.
I desided to modify our circuit for adding shunt registor.
Best regards,
M.Kiniwa
You don't give us any details on what you need for measurement details, like level, accuracy, AC(frequency?)/DC, or isolation requirements. Overall, it's not quite clear what help you are looking for --- there are three ways to convert current to voltage, and if you don't want the shunt resistance method then if AC-current a sense-transformer is viable (and isolated, although their effect reflects as a low shunt resistance), or you can go with a Hall-effect IC: