Hi, pgo, will USBDM support the new KDS ide soon?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, pgo, will USBDM support the new KDS ide soon?

1,007件の閲覧回数
TOMXUE
Contributor II

Hi, pgo:

The new KDS ide is released recently. And will you prepare to support it for USBDM?

BTW, thanks for ypur genie work on USBDM.

Tao

From Tsinghua University

3 返答(返信)

669件の閲覧回数
pgo
Senior Contributor V

Update on this is available:

Using USBDM with Kinetis Design Studio

669件の閲覧回数
pgo
Senior Contributor V

Hi Tao,

I have applied for the BETA download but it is not available at the moment. 

I will have a look when it is available.

PS> You could try USBDM+Eclipse+GNU Tools for an alternative  This works on Linux + Windows.

http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/code_sourcery_install_page.html

bye

669件の閲覧回数
perlam_i_au
Senior Contributor I

In this case you have to ask to USBDM developers, at this moment they have not mentioned nothing regard KDS support but as long as Kinetis devices use the same debugger interfaces (does not matter if you are using CodeWarrior or KDS) I hope USBDM will support KDS soon.

0 件の賞賛
返信