Hi, pgo, will USBDM support the new KDS ide soon?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, pgo, will USBDM support the new KDS ide soon?

1,041 Views
TOMXUE
Contributor II

Hi, pgo:

The new KDS ide is released recently. And will you prepare to support it for USBDM?

BTW, thanks for ypur genie work on USBDM.

Tao

From Tsinghua University

3 Replies

703 Views
pgo
Senior Contributor V

Update on this is available:

Using USBDM with Kinetis Design Studio

703 Views
pgo
Senior Contributor V

Hi Tao,

I have applied for the BETA download but it is not available at the moment. 

I will have a look when it is available.

PS> You could try USBDM+Eclipse+GNU Tools for an alternative  This works on Linux + Windows.

http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/code_sourcery_install_page.html

bye

703 Views
perlam_i_au
Senior Contributor I

In this case you have to ask to USBDM developers, at this moment they have not mentioned nothing regard KDS support but as long as Kinetis devices use the same debugger interfaces (does not matter if you are using CodeWarrior or KDS) I hope USBDM will support KDS soon.

0 Kudos
Reply