Dear all,
I just starting to use the new KEA from NXP and we have a TRK EVB for a KEA8.
I need to emulate the EEPROM in order to store up to 4 bytes of data.
I found the EEPROM emulation driver at nxp.com and downloaded it comes with an API and also found the thread https://community.nxp.com/docs/DOC-328400.
Is there any example of an implementation for the KEA8 for CW? Or AN with an easy approach?
Many thanks in advance,
Marc
Hi
There is EEPROM emulation built in to the uTasker's KEA8 project - either using 512 byte block or 1k area with fail-save swap technique.
A very short video of it in operation is attached (showing swap block switching in internal memory when a parameter save is made).
All code is however compatible with any Kinetis part (KE, KEA, KL, KV, K etc.) and builds with CW, KDS, MCUXpresso, IAR, Keil, Atollic, Rowley, etc...
Regards
Mark
Kinetis: http://www.utasker.com/kinetis.html
Kinetis KEA8:
- http://www.utasker.com/kinetis/TRK-KEA8.html
File and parameter system: http://www.utasker.com/docs/uTasker/uTaskerFileSystem_3.PDF
CodeWarrior: http://www.utasker.com/kinetis/compilers.html#CW10
S32 Design Studio: http://www.utasker.com/kinetis/compilers.html#S32
Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M
For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html