Advice to have quickly a K60 with Ethernet Udp/Tcp and Flash driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Advice to have quickly a K60 with Ethernet Udp/Tcp and Flash driver

ソリューションへジャンプ
804件の閲覧回数
arnogir
Senior Contributor II

Hello,

We need to develop a bootloader for the K60 via the Ethernet (with BootP protocol).

Currently, I'm using the USB bootloader provided by Freescale.

Then, Are they a fast option to dispose (without need MQX) an application with the layer Ethernet to receive and send UDP/TCP frame, and then a Nandflash driver?

I think there are KDSK, with MCUexpresso? Or other? Are they some exempled? (I already use the MQX Ethernet stack with KDS, but not flash driver).

Thank

0 件の賞賛
返信
1 解決策
630件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Maybe you would like to have a look at  FNET Embedded TCP/IP Stack , which provides Ethernet bootloader for K6x chip.

And we also provide an application note for your reference:

https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN4367.pdf 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
631件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Maybe you would like to have a look at  FNET Embedded TCP/IP Stack , which provides Ethernet bootloader for K6x chip.

And we also provide an application note for your reference:

https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN4367.pdf 

0 件の賞賛
返信